(0)| 6/28/2022 9:45 AM | |
|
Posts: 8092 Rating:
|
Hello, Significance of 6 on Simodrive is during the continuous check of the checksum in the program/data memory, a difference was identified between the reference and actual checksum. The cause is probably a hardware fault on the control module. So try by swapping control module from another machine. For encoder alignment, please refer encoder alingment in servo motors post. Hope this helps. |
| 6/30/2022 5:26 PM | |
|
Joined: 10/17/2007 Last visit: 1/14/2026 Posts: 4574 Rating:
|
Your drive is 611A, and servo motor is 1FT5 series Error code "6" is speed control error, very possible due to you lost alignment of rotor position sensor (NOT encoder) during Non- professional servo motor repairing. I suggest you search online to buy a used servo motor (should be the same part # with yours) or send motor to professional servo motor repair shop (best Siemens local shop, but not must be, any servo motor repair shop should be able to do rotor position indicator align for you) I attached basic step file #1 for self-help, to see if you can understand and you have useful devices to do the job yourself, if you think "yes" I will attached another files to do alignment
AttachmentAlignment increatial encoder.docx (862 Downloads) |
Last edited by: nulizhang at: 06/30/2022 18:51:31If you like my comments please |
|
This contribution was helpful to
|
|
Follow us on