7/19/2022 9:55 AM | |
Joined: 7/19/2022 Last visit: 1/6/2025 Posts: 1 Rating:
|
Can I get the project after restore the Psb file to HW? and can I restore the PSB file to another type ? Example: MP377 to TP1200 regard, Ken ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/19/2022 12:49:13New subject after splitting |
|
7/19/2022 9:58 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
the psb can only used with the same type so a change from MP377 to tp1200 is not possible with the PSB file. |
7/19/2022 9:21 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hi, No, you can not get the project from *.psb file. 2nd question already answered. |
Ayman Elotaify |
|
Follow us on