7/14/2022 7:36 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
OK. Sorry my understanding mistake. So yes, you can replace Fanuc motor (refer attached motor data sheet) with Siemens equivalent motor, but need to modify mounting brackets & check the mounting feasibility. Also check what type of encoder does your system needs i.e. incremental or absolute & check Siemens infeed capacity. Equivalent Siemens motor is 1FT6082-1AF71-1xG1 where x = A for sin/cos 1Vp incremental encoder or x=E for EnDAT absolute encoder 2048 S/R. Tech spec of Siemens motor are - Mo - 13 Nm, Nn - 3000 RPM, P - 3.2 Kw, In - 18 Amp, SH = 80 without brake since original Fanuc motor is without brake. Power cable 6FX8002-5CA02-1xx0 xx - length of cable. Siemens LT module which you specified 6sn1123-1ab00-0ca2 is compatible for this motor but check its cooling as it is for external cooling. AttachmentFANUC AiF 12_3000 tech data.pdf (793 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on