9/23/2022 6:55 PM | |
Joined: 8/27/2022 Last visit: 9/23/2022 Posts: 1 Rating:
|
Have a program that was provided by a third party who has fallen off the grid. I have 8 LOGO's that control door access via mag locks. Currently a single door has to provide it's status (open/Closed) to the other 7 door Logo's. It also has to read the other 7 door status. From what I have gathered, each logo can have 8 network connections. Maybe I am using the wrong logic in network mode. When I connect a string from an Output in PLC "A" to an Input on PLC "B" and so on, it turns the input green and adds an IP. Once that has been done 8 times, it tells me that I can no longer add more network connections. Any help would be appreciated. AttachmentUpdated Interlocking Scheme.pdf (436 Downloads) |
9/23/2022 7:41 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
Your PDF is not helpful. Rather show your network project. |
Follow us on