9/25/2022 7:06 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
There are two ways to connect a LOGO! to a Siemens HMI. 1.) By using a HMI connection. The LOGO! can manage only one HMI connection. In this case you must make a connection in both devices. HMI communication since WinCC V11.x (TIA Portal) 2.) By using a S7 connection. Then you need only a connection in the HMI. For this Siemens has no example. But it is my favorite ... |
This contribution was helpful to
1 thankful Users |
Follow us on