10/12/2022 12:31 PM | |
Joined: 9/5/2022 Last visit: 8/13/2025 Posts: 11 Rating:
|
Hello, I have a project where I need more than 8 analog outputs, respectively 10, I am thinking of using LOGO PLC but for this instance it means that I would have to network 2 LOGO PLC, my concern is that in the Modbus address there are only 8 AQ available and even if I can have 8 AQ available for each LOGO PLC, the mapped Modbus addresses are the same for both of them, from 513-520. My question is, how can I have more than 8 different addressees, Or how would I add that differently to the HMI ? Thank you, Raul ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/13/2022 03:51:24New subject after splitting |
|
10/13/2022 3:53 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Logo PLC, more than 8 analog outputs is published within the conference LOGO! - Communication. Jen_Moderator |
Follow us on