(0)| 12/14/2022 1:46 PM | |
|
Joined: 8/8/2022 Last visit: 1/14/2026 Posts: 28 Rating:
|
The max is 20ft/second which will give me a 550hz signal at the output. I am assuming it will scale to GPM for the PID. The PID PV and Set Value are in GPM. then then it controls a valve to adjust the GPM. I am assuming there were calculations that were done but I am not sure what they were or what values were being used. I am trying to get the valve output from the PID to work better. The HSC is 30khz for counting the output of the and they are also using a 1ms counter to track the time elapsed. Attachmentseametrics-ex800-series-insertion-electromagnetic-flow-sensor-instructions.pdf (1341 Downloads) |
Last edited by: mlmartinet at: 12/14/2022 14:05:33Last edited by: mlmartinet at: 12/14/2022 16:15:33 |
|
Follow us on