(0)| 2/1/2023 3:56 PM | |
|
Joined: 8/12/2021 Last visit: 12/10/2025 Posts: 351 Rating:
|
Hi Joanna.S! If I'm not wrong, you just need to not configure the output you are not going to use. Have a look at this manual.
|
|
If this Information really helps, you could use the Rate function |
|
| 2/1/2023 8:22 PM | |
|
Joined: 3/28/2015 Last visit: 1/4/2026 Posts: 727 Rating:
|
Hello, 1-In the H.W configuration of Step7,Deactivate the unused group. 2-If one input of the group is not used,you can Deactivate the Group diagnostics for this group or connect a resistor (1.5K to 3K ohm) between the unused input terminals. |
|
Eng.Mohamed Ibrahim |
|
| 2/2/2023 8:59 AM | |
|
Posts: 31 Rating:
|
Ok perfect! my case is the one from the point 2. So resistor is a solution regardless if it is 4-wires or 2 wires transducer? |
Follow us on