2/9/2023 8:19 AM | |
Joined: 2/28/2018 Last visit: 3/2/2023 Posts: 3 Rating:
|
Hi there; I have crashed node-red while making a dashboard ui. Everything was working fine, then i tried to add a new table with a 'While ' loop, the deploy was continuously runing, so i reboot the IOT2050 advanced (with last example img), and it's no longer possible to open the node red webpage. IOT remains accessible with SSH PuTTY, but when i tried to access directory to erase (rm flows_iot2000.json) the iot reply 'no such directory. I attached a pdf with every feedback even the systemctl status node-red . I'm blocked here if anyone could help....many thanks in advance. Next step i will try to re-install example image, and restart from scratch. Regards Lal AttachmentBrouillons.pdf (497 Downloads) |
Follow us on