(0)| 3/9/2023 2:44 PM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi potretma, As far as I can see from the product description, it does say that it is the direct successor. I share with you the link where you can find it: "6ES5928-3UB12: CPU928B CENTR.CONTR.MOD. F. S5-135U/155U" On the other hand, if you go into the successor product information (in your case 6es5928-3ub21) if you click on 'Delivry release' you will find what you have to keep in mind if you use this as the successor to the previous one (6es5928-3ub12). I also share the link with you: "6ES592828-3UB21: CPU928B Centr.contr.Mod. f. S5-135U/155U" 'Delivery Release' -> 6ES592828-3UB21 -> "CPU 928A and 928B - New Versions with New Catalog Nos." As far as I can see there is no comment on the analogue inputs that need to be taken into account. I hope I have been able to help you with this information and if not I hope someone else can give you more information. Best regards! |
|
If this Information really helps, you could use the Rate function |
|
Follow us on