4/5/2023 12:13 PM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello, you can mix segments and points. Between them, the system interpolation is active, you set in the cam config. 8.3.2 System interpolation (S7-1500T) With system interpolation, the transitions are interpolated according to the interpolation type and the response in the boundary points of the transition segment. The following interpolation methods are possible: https://support.industry.siemens.com/cs/ww/en/view/109812059 8.2.3 Creating the synchronous operation function of the cam with the "LCamHdl" library (S7-1500T)
|
With best regards, |
|
Follow us on