(0)| 5/10/2023 3:56 AM | |
|
Posts: 1 Rating:
|
Hi Guys, I used these codes and it was working for the past 6months. I used these codes in AutoHotKey to automatically download datalogs on daily basis, weekly basis and monthly basis. It was working fine. For the last few days onwards, code is working, but it is downloading as "download" file, but without any extension. If I rename to .csv, inside the file, all the data are available without any error. My problem is that it is downloading as mass data, like weekly and monthly, so only one "download" file is created whenever curl code is running and replacing the same "download" file for the upcoming downloads also. So, ultimately I am not getting the backup at all. Please help me to bring it back. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/10/2023 10:47:59New subject after splitting |
|
Follow us on