5/15/2023 11:43 AM | |
Joined: 4/23/2021 Last visit: 10/29/2024 Posts: 2 Rating:
|
We are also facing the same issue ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/16/2023 07:07:47New subject after splitting |
|
5/16/2023 8:51 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16439 Rating:
|
Hello AutoGen_4584334 Basic information you will find here: https://support.industry.siemens.com/cs/de/en/view/109748099 If you start the HMI Simulation the Runtime will try to connect to the ip that is specified in the HMI connection and it is used the Access Point that is set also in the HMI connection. Which Communication adapter or resource is used you define in the assignment in the PGPC interface settings. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on