(0)| 6/14/2023 7:56 AM | |
|
Posts: 2 Rating:
|
Dear All, We have micro master 430 vfd. I want to run it in both direction i.e Forwad/Reverse. On/OFF command is via terminals and frequency and run feedbacks are via profibus. It is running good but not running in reverse direction. Following are the parameters I set for reverse direction . P1000=6. P2232=0 .. P1032=0 So now what parameters should I set that my pump can run in both directions. PLC setting is OK no one change that. Actually this vfd we send for repair and I didn't save the parameters. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Inamkhan at: 06/14/2023 07:57:33Last edited by: Jen_Moderator at: 06/27/2023 12:38:13New subject after splitting |
|
Follow us on