(0)| 7/30/2023 8:32 AM | |
|
Posts: 26 Rating:
|
Hi, I want to display weekly timer settings in the web gui. If I put 1 timer (cam) in LWE it works fine, fast and can see the changes on the logo display parameter settings. When I copy timer 1 on the web and change the block numbers etc. then the in/off switches for the weekdays are not working anymore for both klocks 1 and 2. The on/off times seem to work though. Attached the project. PS: I don't understand the concept of TagTable in LWE. Isn't that redundant with the parameter VW mapping in LSC ? Attachmentweeklyinweb.zip (469 Downloads) |
Last edited by: Domoticom at: 07/30/2023 08:35:22 |
|
| 7/30/2023 9:32 AM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36467 Rating:
|
I checked it with my LOGO! 8.3. I had no problems with with cam 1 and cam 2. |
Follow us on