(0)| 7/31/2023 3:49 PM | |
|
Joined: 6/11/2019 Last visit: 1/12/2026 Posts: 2721 Rating:
|
Hello Andrus_Saar, Simply build a ramp according to your needs. greeting Ella_68 (translated with Google) |
| 8/1/2023 12:56 AM | |
|
Joined: 10/15/2022 Last visit: 12/24/2025 Posts: 68 Rating:
|
Hi, all. I made "Analog ramp test" program to see how it behaves. I wanted the analog mux to give the analog ramp two speeds. This only worked if the analog ramp was listed first and the analog mux was listed later in the VM table. On the contrary, it didn't work. Only analog ramp D (block B004) works the way I want. Important to know! When simulating program, all ramps behaved the same, only when testing on the real controller (6ED1052-1MD08-0BA1, with firmware 1.83.02) the analog mux was in effect. Could someone can test two controllers linked together where making a speed change in one would affect the ramp speed in the other? Andrus AttachmentAnalog ramp speed test.zip (558 Downloads) |
Last edited by: Andrus_Saar at: 08/01/2023 01:25:48 |
|
| 8/1/2023 3:35 AM | |
|
Joined: 12/18/2014 Last visit: 1/14/2026 Posts: 36449 Rating:
|
As I wrote in my post
I tested it with two LOGO!s. See attached screen video. AttachmentAnalog Ramp Online Test.zip (637 Downloads) |
Follow us on