(0)| 8/16/2023 12:18 PM | |
|
Posts: 11 Rating:
|
Hi apastore, Regarding the APN, Vivo has only this one: zap.vivo.com.br. I tried other DNS servers as you suggested, but it didn't have any effect; the same error persists. I also attempted to use the HTTP request in Node-RED, and that resulted in an error as well. One thing to note is that if I use this SIM card in my cellphone and share its internet connection to my notebook, I can use MindConnect without any errors. I followed the diagnostic commands you recommended, along with some additional commands for further information. When using the 'nmcli' command, I noticed that the Vivo SIM card only displays 'inet6', whereas other carriers show both 'inet6' and 'inet4.' Could this have any influence on the error? The PCIe model is EC25-AU. I'm attaching all the executed commands and other images illustrating the problem.
Attachmentcomandos.zip (449 Downloads) |
Follow us on