8/18/2023 1:06 PM | |
Joined: 7/27/2021 Last visit: 9/11/2025 Posts: 7 Rating:
|
Hi. I am having a problem to go online with my S7-417 5H CPU. I'm using PCS7 V9.1 SP1 and i'm not able to go online neither with HW Config, CFC or NetPro.I am getting the error shown in the file attached. This happened after downloading a few communications (5 comm) with another S7 417 CPUs using the "Download selected connection" tool in NetPro. I have another projects in the MP in which i have no problem to go online. I also tried to retrieve a previous backup but it didn't work. After Reading theS7DOS Error codes, i found it is a Database error. Can anyone help me with this issue, i dont know wether it's a problem with the ES or with the AS (SFC/SFB corrupt). Thanks in advance. EDIT: I do have Ping Responde from the CPU. |
8/30/2023 10:05 AM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Hello, |
Follow us on