9/14/2023 5:48 AM | |
Joined: 3/14/2008 Last visit: 9/17/2025 Posts: 2217 Rating:
|
Hi, Since you are in the PCS7 forum, I assume you have a S7400 controller. Only VC (Virtual Controller) is supported for S7400. See the link below for additional information. |
If I could help you, you can use the RATE button. Thank you. |
|
9/14/2023 10:50 AM | |
Joined: 3/14/2008 Last visit: 9/17/2025 Posts: 2217 Rating:
|
Hi, You can run SIMIT in DEMO mode which has restrictions such as: - Only 45 minutes of runtime and then simulation ends (you can restart it afterwards) - No archiving of projects - VC can be simulated up to 32 in DEMO mode - SIMIT only runs in the S variant, meaning max. 4000 simulation tags - External couplings not allowed VC can be used in DEMO mode You can find all restrictions and license model concept in the SIMIT manual. See chapter 9.1 for the license model and chapter 1.2 about DEMO mode. Also, there is a overview page with all necessary information about SIMIT: |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on