2/20/2023 11:45 AM | |
Joined: 7/19/2022 Last visit: 9/2/2025 Posts: 436 Rating:
|
Hello Nayef Yahya, Microwin is no longer released for Windows 10, only up to Windows 7 as you can see: STEP7 MicroWIN V4.0 + SP8 y SP9 So it is advised to run it under that OS. On the other hand, this message also usually comes if the S7-200 CPU has the "surname" CN. This means that it is from the Asian market and therefore has to put the whole environment in Chinese to communicate with the PLC.
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on