10/31/2023 1:23 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Correct, you only have to adjust the range. Please bear mark, if you have a RTD element, the range to be set is 0-1 Celsius at the driver block. Then you have to make adjustments in the scaling of the MonAnL block that it's scaled to a "normal" range. |
If I could help you, you can use the RATE button. Thank you. |
|
10/31/2023 2:13 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, you can do the change in online mode (test mode), but also with a download change. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on