11/2/2023 5:26 PM | |
Joined: 3/25/2015 Last visit: 8/5/2025 Posts: 124 Rating:
|
Good evening. I have two V90 drives that are mechanically coupled to move a gantry. Both motors are identical and have absolute encoders. I have a S7-1500 CPU1512C and I would like to move both axis simoultaneously using TO object and MC GearIn instructions. Due to the fact that they're mechanically coupled, I would like to add load sharing to them. I've read this article: https://support.industry.siemens.com/cs/document/109794290/ but I don't understand if I can use those functions with TO objects. I've already manage to move both axes with Telegram 3 and IRT with generic GSDML file for V90. Anyone has a suggestion on how to do all this? |
Last edited by: simonspt at: 11/02/2023 17:27:31Kind regards |
|
11/2/2023 6:33 PM | |
Joined: 7/7/2010 Last visit: 9/12/2025 Posts: 16094 Rating:
|
If it is possible to get them to act as coordinated axes with a regular S7-1500 PLC, you will definitely want to look into PN IRT and ISOchronous mode: Isochronous mode (siemens.com) That PDF includes a link for parameters affecting ISO performance at the end of the document.
Attachments71500_isochronous_mode_function_manual_en-US_en-US.pdf (476 Downloads) |
Last edited by: Jen_Moderator at: 11/03/2023 09:09:26PDF added from link. science guy |
|
11/3/2023 11:40 AM | |
Joined: 3/25/2015 Last visit: 8/5/2025 Posts: 124 Rating:
|
When you say "coordinated axes" you mean "TO Synchronous" axes? If I use SIEMENS Telegram 102 (IRT) and MC instruction GearIn, would it be possible without upgrading the CPU to a T model?
|
Kind regards |
|
Follow us on