10/5/2022 6:18 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, this will work, but you have to use bit 0-7 in the chronological order so connect the following signals to the BO_W block: I12.0->IN0 I12.1->IN1 I12.2->IN2 I12.3->IN3 etc. From you printscreen, I don't know if you have connected IN0, IN4 etc. because it's not visible. But you have to be sure that those bits are defined as the Status word... Can't you replace the Basic Type 2 module for another one that reads Word? |
If I could help you, you can use the RATE button. Thank you. |
|
10/6/2022 11:25 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, You can address the bit range as a word in the symbol table as well. When using the word address in the CFC program, it basically starts reading the word at I12.0 and reads out the whole area I12.0-I13.7. So that is possible as well, even if the module is shown in bits. |
If I could help you, you can use the RATE button. Thank you. |
|
10/10/2022 10:31 AM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Hello Cristian, SIMOCODE PRO V (Profibus) - Addresses will be coming in Word irrespective of Basic Type 1 or Basic Type2. No need to convert the bool addresses to word and use it in program!. You can directly use the address as IW0 (If the addresses are starting from I0.0 in Hardware configuration of SIMOCODE PRO V PN). Please find the attached Zip file of configuration. I hope it clarifies your doubt! AttachmentSIMOCDE_SS.zip (633 Downloads) |
11/21/2023 12:59 PM | |
Joined: 4/6/2021 Last visit: 9/4/2025 Posts: 1 Rating:
|
I Have made some steps to show how to get a word adress and symbol reference to the Simocode Profinet, this because it took me sometime to get it right.
AttachmentSimocode Adress from Bool to Word.zip (361 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on