11/30/2023 9:14 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, With online you mean opening data blocks online, creating VAT tables and monitor signals and edit ethernet nodes functionality? These actions can be done without consequence, but user is responsible. Simatic Manager works in PCS7 mode in PCS7 installations and some restrictions apply such as downloading separate data blocks is not possible. User can copy the online blocks folder from the CPU and possibly delete blocks online. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on