12/8/2023 8:23 PM | |
Posts: 1 Rating:
|
Tnx, But is there any way to use this timer for transition? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/11/2023 09:50:36New subject after splitting and Quote from initial Topic added |
|
12/11/2023 10:20 AM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Hello, |
12/11/2023 12:56 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, In a SFC type, you can create a timer under Characteristics -> Timers and use it in the step to activate and to set them mode + timer value. The timer characteristic is based on block: TIMER_P. You can use the timer to evaluate the transition, you can see it count down if you use the PTIME value. See attachment. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on