11/23/2023 7:32 AM | |
Joined: 8/31/2022 Last visit: 2/10/2024 Posts: 1 Rating:
|
Hello Tautom I have the same issue as you did with PCS7 V9.1 SP2. The only difference is that instead of a WinCC Ref project is that I have a WinCC Standby. Could you please explain how to access the SQL Databank and how to change the value there since I am not familiar with how to do that. Kind regards Christiaan van der Westhuizen ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/23/2023 11:40:58New subject after splitting Last edited by: The Helping Hand at: 11/23/2023 11:41:51 |
|
11/24/2023 12:24 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Maybe you can share a couple of print screens of your setup. What kind of setup do you have? We can try to solve this using the normal way instead of "hacking" in the SQL database. That is not something that should be done. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on