12/27/2023 1:08 PM | |
Posts: 1 Rating:
|
Hi, i have serious troubles to get the cpu 410-5h into my pcs7 project. The cpu is missing in the hardware catalog. There are a few threads about this topic in this forum, but it seems no one has a full solution yet, so i decided to start this thread. My Problem: When i open a given project the cpu can not be loaded and is only display by a yellow missing box. When i open the hardware, i get a message that the used cpu is not installed and i shall get the right "Optionspaket" for it. I also can not find it in the hardware catalog. What i've tried: I used a brand new pc running Win10Pro and installed PCS7 9.12. In my opinion this should already include the CPU 410-5H but obviously not. Then i have downloaded and installed all possible HW-Updates from the web (with hw-updates inside pcs7) . No changes. Finally, i tried to install F-Systems but didn't help. I attached 6 pictures containing errors, version numbers used by me and installed updates zipped. Can anyone help me out? I've already spent way too much time trying to find a solution. Thanks! All the best d.e Attachmentimages.zip (283 Downloads) |
Last edited by: The Helping Hand at: 12/27/2023 15:21:25Text formatting optimized |
|
12/27/2023 5:39 PM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Hello, Siemens have tested and released for below version of Microsoft OSs. I am not sure, You can give try by installing UC03 on top of PCS7 V9.1.2 and check SIMATIC PCS 7 V9.1 SP2 Software Updates
|
Follow us on