1/2/2024 12:16 PM | |
Joined: 1/2/2024 Last visit: 7/12/2025 Posts: 20 Rating:
|
sir i need help !!! I have an MP277 panel, i'am talking about a real physical panel not the panel in tia portal. I downloaded a small program with a start button and an indicator. the program works perfectly but i don't know how to get out of the simulation inside my panel to the windows view. The panel has no buttons and i forgot to make a button with a "Runtime Stop" to shut the simulation and get back to windows I have cut the power then got it back, the panel starts and windows system appear but it immediatly got back to the simulation. i'am frustrated and don't know what to do. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/02/2024 12:49:31New subject after splitting To reach level ONE THOUSAND... It's hard work !!! |
|
1/2/2024 2:59 PM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi AutoGen_5311751, Have you tried doing a factory reset? This way you would delete the project that is loaded in the panel. Regarding MP277 factory reset settings, please refer to the link below for more details: "How do you do a SIMATIC HMI operating system update (firmware update, OS update) on operator panels or perform a "Reset to factory settings"?" You will need WinCC, WinCC Flexible, or Prosave to do reset to factory or download image/ OS update for MP277. If you do not have WinCC/WinCC flexible, you will need Prosave, which is free to download in the link below: "Servicetool SIMATIC ProSave" Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on