(0)| 2/19/2024 10:12 AM | |
|
Joined: 3/14/2023 Last visit: 3/26/2024 Posts: 3 Rating:
|
Good evening everyone. I have a problem with CPU 315-2 DP. Suddenly it stopped working and the SF LED is flashing red, while all the others are off. The MMC card inside is practically dead, it is not detected by the reader. I therefore inserted another MMC that I had available but the CPU continues to flash red. I read on the internet that it could be the CPU firmware that is damaged but unfortunately I can't find a way to communicate with the CPU. If I try to connect with STEP 7 I cannot detect the CPU and no accessible node. As if it wasn't connected. What do you think I could try to do? Thank you all for the support Attachment427701668_1545116629672497_2876156213174226042_n.avi (555 Downloads) |
Last edited by: The Helping Hand at: 02/20/2024 08:36:21Text formatting optimized |
|
| 2/19/2024 12:23 PM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
I have been reviewing the CPU 315-2 DP manual and the SF Led flashing red indicates: 'Hardware fault or software error'. You can find this information in the following manual (Page 48): [snip] Therefore, you can try to do a factory reset and install the latest firmware available. I share the following links that may help you: "How do you reset a SIMATIC S7-300 CPU and MMC (default reset or overall reset)?" "Firmware updates for CPU 315-2 PN/DP (6ES7315-2EH14-0AB0)" Best regards! Attachments7300_cpu_31xc_and_cpu_31x_manual_en-US_en-US.pdf (1049 Downloads) |
Last edited by: The Helping Hand at: 02/20/2024 08:35:41File attached from link. If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
Follow us on