5/2/2024 1:43 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, you find the parameter in the function diagram. So you can evaluate the differences. https://support.industry.siemens.com/cs/ww/en/view/32441736 I would use standart telegram like Tel.1 and do a telegramm extension to connect further parameter. So it is possible to use function blocks like SinaSpeed. https://support.industry.siemens.com/cs/ww/en/view/109485727 You can make a script file, when using Starter to do the parameter connections a second time. |
With best regards, |
|
5/8/2024 1:30 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, with Starter you can use Script files, for writing parameter values. https://support.industry.siemens.com/cs/ww/en/view/75163088 It is necessary to provide the bits of the used telegram. You can copy the relevant bits from your structure to the used telegram. |
With best regards, |
|
Follow us on