(0)| 6/24/2023 12:13 PM | |
|
Posts: 1 Rating:
|
is there possibility to modify this program? example: pump1 is ON when pressure is -0.5bar and it stops when pressure is -0.6bar If pump 1 can not reach pressure of -0.6, then pump 2 starts at -0.4 bar and they both switch OFF at -0.6. If pressure is rising, then pump 3 needs to start at -0.2 bar and all three stops at -0.6 bars. And as I already mentioned, they need to change over every 10 hours, so first 10 hours pump 1 is MASTER then next 10 hours pump 2 and so on. this is program so far what I did ------------------------------------------------------------------------------------------ Attachmentsewage 2023.zip (1808 Downloads) |
Last edited by: Jen_Moderator at: 06/26/2023 10:05:26New subject after splitting |
|
| 6/24/2023 5:59 PM | |
|
Joined: 6/11/2019 Last visit: 1/18/2026 Posts: 2729 Rating:
|
hello spavic7, I'm assuming that you mean that if the pressure continues to rise despite pump 1 being in operation, pump 2 will switch on. It looks as if you have integrated a failover in your program. This makes little sense to me, however, since the staggering of the pump switch-on points means that the next pump works the same way up to the switch-off point. Unfortunately, the program is quite confusing due to the separation of the connections. So a suggestion from me. greetings Ella_68 (translated with Google) Attachmentsewage 2023 mod.zip (983 Downloads) |
This contribution was helpful to
|
|
| 5/21/2024 8:55 AM | |
|
Posts: 8171 Rating:
|
New question published by pnatarajan0107 is split to a separate thread with the subject Convert Logo program to TIA program. Best regards |
Follow us on