(1)| 3/15/2024 11:56 AM | |
|
Joined: 12/18/2014 Last visit: 1/15/2026 Posts: 36457 Rating:
|
Solar Positioning Algorithm (SPA) Library for SIMATIC S7-1200 / S7-1500The "Solar Positioning Algorithm (SPA) Library" provides the calculation of the actual position of the sun for any location on Earth. The position of the sun is given in relation to the angles Azimuth and Zenith. Which can then be used to calculate the right angle for the Tracking movement This library can be universally used with the following controller:
|
This contribution was helpful to
|
|
| 5/22/2024 5:14 PM | |
|
Joined: 5/22/2024 Last visit: 2/7/2025 Posts: 2 Rating:
|
Hello, don't you also use one or two sensors per axis, in order to refine the placement of the solar panel?
|
Follow us on