(0)| 5/24/2024 7:33 AM | |
|
Joined: 10/29/2020 Last visit: 11/29/2024 Posts: 4 Rating:
|
Hello everyone, I am currently working on a project, where we are using Sinamics S120 (CU320-2PN) to control 6 Axes, I am also using a #MC_Measuring for one of the axes. This is set to fault 755, and the axis in question is set to fault 7565. Also, command word GS_ZWX = 0. Resting the axis and resetting the #MC_Measuring function is done directly from a #MC_reset. according to several documents colsulted to try to understand, the cause of the program is well the encoder, except that it recuperates well the speed and the position of my axes. attached are a few photos of the situation, if anyone can help me please.
Best regards, AttachmentS120.pdf (779 Downloads) |
Follow us on