(0)| 6/25/2024 11:28 AM | |
|
Joined: 7/19/2022 Last visit: 1/14/2026 Posts: 436 Rating:
|
Hello AutoGen_2417961, If it is necessary to update Windows to 2022, it will be necessary to go to STEP 7 V5.7 since it is the version released to function correctly. At the program level, it should not cause any major problems unless there is a specific component that also requires an update when upgrading to STEP 7 V5.7. You can try first with a trial version: STEP 7 V5.7 / S7 GRAPH V5.7 / S7 SCL V5.7 / S7 PDIAG V5.7 / STEP 7 Professional 2021 Trial Download |
Last edited by: Jen_Moderator at: 06/26/2024 08:28:13Link optimized. If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
Follow us on