(0)| 6/26/2024 8:45 AM | |
|
Joined: 11/21/2020 Last visit: 8/26/2025 Posts: 213 Rating:
|
Hi, Why are all 4 LEDs constantly ON, I don't use module in current program at all?
|
| 6/27/2024 5:56 PM | |
|
Joined: 5/6/2022 Last visit: 1/14/2026 Posts: 589 Rating:
|
Hi milos23, If you are not currently using the channels, I recommend checking what is indicated in the manual: "Unused voltage input channels should be shorted." Unused current input channels should be set to the 0 to 20 mA range and/or disable broken wire error reporting. Inputs configured for current mode will not conduct loop current unless the module is powered and configured. Current input channels will not operate unless external power is supplied to the transmitter. Best regards! |
|
If this Information really helps, you could use the Rate function |
|
Follow us on