7/3/2024 11:19 AM | |
Joined: 6/1/2024 Last visit: 9/16/2025 Posts: 21 Rating:
|
Hy everyone specially experts I have made a report in WinCC explorer 7.5 as you can see here in the video: WinCC Reporting| Archive Start/Stop| Report Print |WinCC Explorer7.5 (youtube.com) as you can see in video, so I want only data from 1:49:05 to 1:49:16 (as an example) Problem: "The Problem is when I print data it also prints previous data, but I want data only between "Start and Stop" button. I hope you understand is there any script or some settings which can help me I need: I want to print data when click on start and stop even it is 10 times. Every time data should be between start and stop button. hussnaincheema125@gmail.com that is my Gmail if someone has done advance level reporting, he/she can share here Regards, |
Last edited by: AutoGen_5448484 at: 07/03/2024 11:22:23Last edited by: Wit_Moderator at: 07/04/2024 13:36:25Video embedded Last edited by: AutoGen_5448484 at: 07/05/2024 12:29:10 |
|
Follow us on