9/10/2014 11:00 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating:
|
Hi gunnerabzuaki, with which WinCC version do you have this effect? Best Regards, Healthcheck |
Grundkurs/Systemkurs WinCC V7: |
|
7/19/2024 6:25 AM | |
Joined: 8/28/2017 Last visit: 5/23/2025 Posts: 7 Rating:
|
Hello Murof, I use TIA Portal and WinCC Professional V17 Upd 4. The online trend control in trend page has a 1920x780 layout with default ttle style and toolbar visible, whilst the control hardcopy in report has a 1050x400 layout (1050 is due to A4 page format). I suppose it is a scaling issue, in fact if I set the trend layout to 1050x400 and remove title and toolbar then the report printout is perfectly corresponding to trend page. It seems that only the ruler is not scaled; even though the attached images do not contain logged values, I confirm that they are correctly scaled. Best regards Attachmentruler.zip (334 Downloads) |
Follow us on