(0)| 8/6/2024 10:09 AM | |
|
Joined: 6/24/2013 Last visit: 11/14/2025 Posts: 1696 Rating:
|
Sketch of flying cutter sequence attached it uses external cut finished pulse. Clutch drives cutting blade and when cut is done sequence resets clutch and starts braking cut inhibit is input for example from NDT to inhibit cut on product with open seam which would damage cutter. next cut position refers to position on master axis (material encoder) S7-1500T required!!! AttachmentCut_Seq.pdf (701 Downloads) |
| 8/7/2024 12:44 PM | |
|
Joined: 10/11/2006 Last visit: 1/5/2026 Posts: 6064 Rating:
|
Hello, MC_GearIn is "position gearing" like MC_GearInPos. The main differnce is that MC_GearIn enables gearing immediately. Best way is to move the following axis to the desired position and then do a MC_GearIn during standstill. The difference is described detailed in the manual. 6. Gearing (S7-1500, S7-1500T) https://support.industry.siemens.com/cs/ww/en/view/109817888 |
Last edited by: Technology Team at: 08/07/2024 12:45:09With best regards, |
|
Follow us on