8/10/2024 7:47 AM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
Hi, In the following link you can find the released modules for PCS7. Please select the correct version before opening the document. Siemens is using the CPU410-5H as the only controller used for PCS7. This CPU can handle everything like standard operation or redundant setup, with/without safety functions. Before the CPU410-5H there were a lot of CPU's like CPU414, 416, 417, 417 redundant and so on. With the CPU410-5H they rely on only one controller. It's the best CPU, but you can scale it according to your needs in the form of AS PO. If your application become larger, you won't need to replace the CPU for a bigger one. You already have it with the 410. The only thing is that you increase the amount of AS PO in the CPU. The "H" in the name means high availabilty and does not mean it's a CPU with redundant capability only. |
Last edited by: Moderator_Lan at: 08/12/2024 07:39:33link optimized If I could help you, you can use the RATE button. Thank you. |
|
8/16/2024 8:33 AM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
Hi, See below my answers in bold
You can find all info about the CPU410-5H/E in the following manual: Process automation with the SIMATIC PCS 7 CPU 410-5H controller |
Last edited by: Moderator_Lan at: 08/16/2024 09:00:36links optimized If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
8/19/2024 1:44 PM | |
Joined: 4/15/2019 Last visit: 8/1/2025 Posts: 3 Rating:
|
Thank you so much mister, appreciated. |
Follow us on