(0)| 11/4/2021 4:31 PM | |
|
Posts: 2 Rating:
|
Hi, my IOT2050 with the example-image, i want to use WiFi and Bluetooth. i have an Intel AC-9260NGW with M.2 A-E-Key, an Intel AC-7265 with M.2 A-E-Key, a SparkLAN WPET-236ACN(BT) with Mini-PCIe and a WCBN608AH with Mini-PCIe from my old Lenovo Laptop. Both Intel Module were connected via an Adapter like this one: conrad.de and i got only Bluetooth working. The SparkLAN WPET-236ACN(BT) is directly connected to the IOT and there is also only Bluetooth available. But with the old Lenovo Module WCBN608AH, i got access to WiFi and Bluetooth. Is there any newer WiFi+Bluetooth 5.X Module, that i can use? Maybe one with Mini PCIe Connector? thanks in advance |
Last edited by: haoning at: 11/04/2021 16:32:20 |
|
| 11/8/2021 1:12 PM | |
|
Joined: 4/28/2015 Last visit: 1/15/2026 Posts: 3345 Rating:
|
Hi, seems that the current revision of the IOT2050 has a hardware bug regarding the reset pin of the mPCIe interface. I guess that is the reason for the not dettected WiFi interface. Development was testing this with the new hardware revision (PG2) of the IOT2050 and this works with the Intel 9260. I cannot recommend a card with BT and WiFi, because we haven't tested / listed working cards. We tested a USB BT adapter, maybe you can use this? An overview of the devices we tested can be found here. Best regards! |
Last edited by: bergmanu at: 11/08/2021 13:13:40Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
|
|
Follow us on