(0)| 9/18/2024 3:41 PM | |
|
Posts: 4 Rating:
|
yes, i understand this, but… in Python which are the memory address to use...correlated to 0-849? for example in the Python instructions: ### Digital Mark plc.write('V1104.0', 1) << write a true (1) to bit of the first digital Mark M1, and the memory address is V1104.0 ### Analog Mark plc.write('VW1118', 32767) << write an integer (32767) to first analog Mark VW1118 position (2 bytes) Memory 1104 for Digital Marks (bit) 1118 for Analog Marks (integer) see attached table... and for 0-849 directions of mapping table? i don't want to write a mark, i want to write one of the 0-849 positions (memory address) of the mapping table to use in like parameters dinamically thanks a lot AttachmentLOGO! 0BA8 Reserved VM addresses.pdf (618 Downloads) |
Follow us on