(0)| 3/31/2021 8:05 AM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Dear jotey, Status and error display of the CPUregards sancruz |
|
Feedback appreciated, please rate |
|
| 9/26/2024 7:46 AM | |
|
Joined: 3/10/2022 Last visit: 7/27/2025 Posts: 4 Rating:
|
Hi thank you for the response The CPU for which i face this issue is primary CPU of the 1517H bundle I have attached the pictures of the current condition of the CPU yes, we removed the CPU to desk and energized separately with 24V PS the following conditions experienced 1. CPU powers up and displays "CONNECTING..." 2. can't access the device via TIA portal 3. can't ping the Device IP address 4. RUN/STOP LED blinks orange continously 5. can't access any details in the diagnostic buffer, overview, settings and Memory card and any other options tried to update the firmware via memory card v3.1.4 but no response from the CPU
AttachmentRedundant cpu error.zip (419 Downloads) |
Follow us on