5/22/2019 12:21 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating:
|
Respected all, I need script (VB) for redundant communication with H system from my SCADA PC station. Addresses are as given below-- H master- 192.168.0.1 H standby- 192.168.0.2 PC station- 192.168.0.10 There is single inbuilt ethernet port on PC station. See also attached HW cnfg. AttachmentHsys.zip (298 Downloads) |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
10/4/2024 10:42 AM | |
Joined: 8/3/2009 Last visit: 9/3/2025 Posts: 16322 Rating:
|
This is only a S7 Project in the attachment. It would help us if you post more information about your question. If you need more help in Software Redundancy connection then check the Manual: https://support.industry.siemens.com/cs/ww/en/view/109818193/2454306827 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on