9/18/2023 5:11 AM | |
Posts: 1 Rating:
|
I can not setup STARTER 5.5 HF1, The fault is: The installation files integrity check was not succesful! Details see log file CheckIntegrit.log Setup will be aborted without installation! Note: With silent installations, the SetupMode.ini file must be copies into another directory and change. The Setup.exe must then be called with the <path>\SetupMode.ini parameter. PLEASE HELP ME! THANKS
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/18/2023 11:48:19New subject after splitting |
|
10/20/2023 2:55 AM | |
Joined: 6/10/2020 Last visit: 4/15/2024 Posts: 1 Rating:
|
Very helpful, thanks~ |
10/22/2024 12:10 PM | |
Posts: 2 Rating:
|
you must unzip the 3 Zip files into a single folder, then run the installer saludos LGR |
This contribution was helpful to
5 thankful Users |
Follow us on