(0)| 10/25/2024 1:51 PM | |
|
Joined: 9/29/2024 Last visit: 11/15/2025 Posts: 2 Rating:
|
Hello- I am looking for some help with conversion of our Siemens system (Windows 2000) from physical to virtual machine. I know that most of you did this 10-12 years ago, and I am rather late in the game here... I am dealing with a 20-year-old PC that has somehow managed to survive just fine all this time (and is currently still working!) Trying to get it replaced before it eventually gives out! I am very experienced in IT, but have little to no experience with the Siemens hardware. The card in the ancient PC is a 6GK1561-1AA00. Besides the fact that I need to keep the old machine intact as a backup until it actually dies, the new PC is fanless mini, and has no slots to try the card out. I am thinking we just need to get a USB Simatic Net module, such as the 6GK 1571-0BA00-0AA0, and that after that we should be pretty much golden. Wondering if there is anything special in the software needed to recognize it's coming from USB instead of a card and also if there are any compatibility issues with WIndows 2000 and this (or other model) USB solutions. If anyone has any other tips or pitfalls to look out for I'd really appreciate it. I feel like it should all work once we get the Simatic Net communications going and I have ensured the other serial ports are properly mapped to the physical ports on the new machine, but if one of y'all with experience in this can clue me in, that would be awesome This is a critical system on a 50m boat and I know once we get this working with a VM, we don't have to worry about PC hardware failing any more!
------------------------------------------------------------------------------------------ |
Last edited by: TechnoGurus at: 10/25/2024 13:54:14Last edited by: TechnoGurus at: 10/25/2024 13:54:54Last edited by: Moderator_Lan at: 10/25/2024 13:57:43New subject after splitting Last edited by: TechnoGurus at: 10/25/2024 18:13:19Last edited by: TechnoGurus at: 10/25/2024 18:14:12 |
|
Follow us on