(0)| 11/2/2024 6:42 AM | |
|
Posts: 7 Rating:
|
IOT2050 FS:09 1P6ES7647-0BA00-1YA2 Hi guys , I've connected my IOT 2050 to my pc through ethernet cable and set my computer's ip range to 192.168.200.... but istill i cannot connect to device throuth putty. ive also tried flashing service stick with blena etcher to my usb flash disk and connecting with hdmi to hdmi-D cable but still i cant see any thing on my monitor . i dont know whats the problem that i cannot do any thing with this device! also tried flashing an example image to an micro SD card and too many trys but still cannot connect to the device or seeing anything on display. when i turn on the device or push the reset button the stat LED is power on for some seconds and then it goes off . hey guys , help me to use this device :( ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 11/04/2024 08:51:58New subject after splitting |
|
Follow us on