11/4/2024 11:19 AM | |
Joined: 3/12/2015 Last visit: 9/1/2025 Posts: 555 Rating:
|
Good morning forum, Im having a lot of dificulties accessing a machine that i am trying to fix. Basicly i have an 840D SL (PLU50.3) with a ncu710.2 which im trying to see the ladder diagram from the plc but all i can do is download to a usb the plc.arc from the control because when i try to connect my step 7 i can see the ncu with its ip address but it cant connect. I havent used step 7 in a long time and i now have the `new´ version V5.7 SP2 of step 7 Attached are photos of when i try to connect and the plc.arc AttachmentPLC.zip (117 Downloads) |
11/4/2024 11:26 AM | |
Joined: 3/12/2015 Last visit: 9/1/2025 Posts: 555 Rating:
|
screenshots of attempt |
Follow us on