(1)| 11/6/2024 5:40 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, Create a Control Value in the first SFC type and set the value to 1 somewhere you want and update the instance(s), connect the CV to a command of the second SFC instance like Start/Complete or create a Process Value in the second SFC type and use that PV to set a internal command. |
Last edited by: Oreca at: 11/06/2024 17:42:44If I could help you, you can use the RATE button. Thank you. |
|
Follow us on