(0)| 10/31/2024 4:05 PM | |
|
Joined: 6/5/2009 Last visit: 1/12/2026 Posts: 158 Rating:
|
Hello Experts, I installed PCS7 v9.1 SP2 on laptop for the benefit of learning Simatic Batch and practicing PCS7. After creating a PCS7 project and going by text book chronology of configuration of batch project, I noticed that Simatic batch was working and was able to add materials, create recipes and create orders. I am, however, unable to enable formulae and Libraries on my laptop. I am unable to enable the setting for from project settings for using them. When I click on default setting, it gets enabled, however it does not appear on the tree view. So I restarted simatic batch and to no surprise, the options were disabled in the project settings. I've attached screenshots of the same with the post. Please do advise on what's needed to be done. Regards AttachmentBatch.zip (190 Downloads) |
Follow us on