8/2/2019 4:44 PM | |
Joined: 12/24/2015 Last visit: 3/2/2023 Posts: 19 Rating:
|
Dear hdhosseini , hope you are doing well , I am trying to simulate 2 cpu via prifibus , simple program using SFC14/15 , but there is no data exchange when using PLCsim ! , asking if SFC14/15 working with PLCsim ? or there is something wrong ? the project file I used is from this article .. DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 V5.3
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/05/2019 06:43:49New subject after splitting |
|
11/7/2024 9:21 AM | |
Posts: 1 Rating:
|
Please can you tell me why you can't use i_put/i_get or i_send/i_rcv in this situation ? What's the difference between SFC14/SF15 and these "i" fonctions ? |
Follow us on